PLUG IT IN, WALK AWAY

At Grundfos, we believe in making the complicated seem simple and innovative technology intuitive.

The AUTOADAPT function reflects this philosophy. It expands the benefits of electronic speed control and makes the pumps even easier to install. With AUTOADAPT, the pump constantly analyses the system it's in and learns from it.

WHAT IS AUTOADAPT?

Developed and patented by Grundfos, AUTOADAPT serves several purposes.

  • Taking variable speed control to the next level
  • Making sure the pump fits the system - all by itself
  • Achieving perfect comfort with minimal energy consumption

NEW IMPROVEMENTS

The AUTOADAPT function in ALPHA2 is the second generation of the well-known and recognised functionality that our customers know from the MAGNA range. The AUTOADAPT setting is the ideal choice for more than 80% of all systems.

This second generation of AUTOADAPT for ALPHA2 offers two distinct improvements:

  • It does not need to reach the maximum pump curve before it adapts to the requirements of the heating system
  • It allows the pump to adjust the proportional pressure curve both up and down

Electronic speed control

Grundfos electronically controlled pumps (E-pumps) are able to deliver intelligent speed control. We've integrated a frequency converter to automatically adjust pump speed to suit demand, which regulates pressure in the system.

Known as proportional pressure, this means you get only the pressure you need.

Rather than running at a fixed speed all the time, Grundfos E-pumps operate on a proportional pressure curve. This makes them far more efficient than standard three-speed pumps.

Speed control responds to changing conditions

The heating demand of any room is influenced by several factors. These include outside temperatures, levels of sunlight, overall activity, and other heating sources.

A speed-controlled pump automatically adjusts its output to changing demand. This lets it meet thermostat settings with the minimum amount of power.

Standard pump - full speed all the time

Standard three-speed pumps run at a fixed speed all the time, regardless of the actual heating demand. That's like driving a car at full throttle and only using the brakes to control your speed.

This means that the pump builds up pressure even when it is not required, which causes noise in the system and wastes energy.

E-pump - much more efficient

A Grundfos E-pump never generates unnecessary pressure. Continuing the car comparison, an E-pump removes the foot from the throttle to slow down and it works out when it can slow down by itself.

The result? A significant reduction in power consumption. Electronically controlled pumps are A-labelled, which means savings of up to 80% compared to typical (D-labelled) pumps. Under normal circumstances, it only takes the end user about two years to recoup the initial extra investment. Combined with Grundfos' reputation for superb quality and reliability, this means considerable savings for many years to come.

OPEN THE SPEED CONTROL WINDOW

HOW DOES IT WORK?

An ALPHA2 on AUTOADAPT automatically searches for the lowest possible head to meet system requirements. It will continuously find the setting where optimal comfort meets minimal energy consumption.

REFERENCE SETTINGS

Set on AUTOADAPT, ALPHA2 starts at a factory pre-set reference duty point on a reference curve. This proportional pressure curve is positioned in the centre of the AUTOADAPT regulation area.

From the pre-set reference duty point, the pump will immediately start to analyse the heating pattern. If the actual duty point deviates from the reference duty point over time, the pump will automatically adjust its performance accordingly.

In other words, if the requirement of the heating system exceeds the reference duty point, the pump will choose a higher proportional pressure curve. Should the requirement be lower, a lower curve will naturally be chosen.

NEW REFERENCE SETTING

When changing the proportional pressure curve setting to adapt to the requirements of the heating system, AUTOADAPT automatically sets a new reference duty point. From the new setting, the process starts over again: AUTOADAPT will continuously adapt to changes in the heating pattern.

REGULATION INTERVALS

When changing the proportional pressure curve setting to adapt to the requirements of the heating system, AUTOADAPT automatically sets a new reference duty point. From the new setting, the process starts over again: AUTOADAPT will continuously adapt to changes in the heating pattern.

EXPLORE THE ALPHA2

INSTALLERS & END USERS

From experience and several market studies we know that the majority of installers never identify the specific details of the heating systems in which they install circulator pumps. Consequently, they find it hard to select the right pump for the system and perform correct setting.

With ALPHA2, the installer can install the pump, select AUTOADAPT, and move on, rest assured that the pump will adapt to the system and automatically select the optimal setting.

End users want to save money on their electricity bill, reduce their share of CO2 emissions, and a reliable pump that guarantees optimal comfort. And ALPHA2 does exactly that, better than ever before.

ALPHA2 TECHNOLOGY

ALPHA2 is filled to the max with sophisticated technology. Get all the technology details by browsing an ALPHA2 pump from the outside to the inside.

EXPLORE THE ALPHA2 TECHNOLOGY

MAGNA TECHNOLOGY

MAGNA is filled to the max with sophisticated technology. Get all the technology details by browsing a MAGNA pump from the outside to the inside.

EXPLORE THE MAGNA TECHNOLOGY

COMFORT AUTOADAPT PM TECHNOLOGY

Get all the innovative features and technology details of the COMFORT AUTOADAPT PM by browsing the pump from the outside to the inside.

 

EXPLORE THE COMFORT TECHNOLOGY